/content/ess/us/en/search-results.html

Honeywell Technology Helping To Produce Sustainable Aviation Fuel With Lower Cost And Waste

Honeywell Technology Helping To Produce Sustainable Aviation Fuel With Lower Cost And Waste

  • Latest technology expands Honeywell’s portfolio of offerings to help meet growing demand for renewable jet fuel
  • DG Fuels to deploy new Honeywell technology in its SAF production plant

CHARLOTTE, N.C., April 24, 2024 – Honeywell (Nasdaq: HON) today announced its hydrocracking technology can be used to produce sustainable aviation fuel (SAF) from biomass, helping to make sustainable aviation fuel (SAF) that is 90% less carbon intensive than traditional fossil-based jet fuels1. The new technology produces 3-5% more SAF2,3 enables a cost reduction of up to 20%3,4 and reduces by-product waste streams as compared to other commonly used hydroprocessing technologies.

Honeywell’s Fischer-Tropsch (FT) UnicrackingTM technology takes liquids and waxes from processed biomass – including leftovers from crops, wood waste or food scraps – and can be used to produce SAF that complies with the strict standards of the aviation industry and with a lower environmental impact. This innovation demonstrates Honeywell’s alignment of its portfolio with three compelling megatrends, including the energy transition.

“As demand for SAF continues to grow, the aviation industry is challenged by limited supplies of traditional SAF feedstocks such as vegetable oils, animal fats and waste oils,” said Ken West, president and CEO of Honeywell Energy and Sustainability Solutions. “When combined with the existing Fischer-Tropsch process, our new technology will expand the feedstock options available in the industry to sources that are more plentiful, ultimately helping improve our customers’ ability to produce SAF.”

Recently, DG Fuels selected Honeywell’s FT Unicracking technology for its biofuels manufacturing facility in Louisiana – the largest in the world for making SAF from the FT process – that will produce 13,000 barrels of SAF each day when it begins operations in 2028.

“Using Honeywell's advanced technology, DG Fuels will supply enough fuel for more than 30,000 transatlantic flights every year, contributing significantly to reducing the carbon emissions of global air travel,” said Michael Darcy, CEO of DG Fuels. “This is a big leap forward in supporting the airline industry's goal of reaching net zero carbon emissions from international aviation by 2050.”

Honeywell helped pioneer SAF production with its EcofiningTM process, which has been used to produce the fuel commercially since 2016. The company now offers solutions across a range of feedstocks to meet the rapidly growing demand for renewable fuels, including SAF. In addition to Honeywell Unicracking and Ecofining, Honeywell's renewable fuels portfolio includes Ethanol to Jet technology and eFining™, which converts green hydrogen and carbon

1Carbon intensity is based on ICAO CORSIA default lifecycle emissions values for CORSIA-eligible fuels, Table 1 - agricultural residues and forestry residues. Corsia Eligible Fuels - Life Cycle Assessment Methodology - Version 5 June 2022.

2By utilizing proprietary SAF selective Honeywell UOP hydrocracking and hydro-isomerization catalysts.

3By utilizing a Honeywell patent pending process configuration.

4Based on internal UOP cost (Estimated Erected Cost) analysis that compares a typical configuration with the patent pending configuration.

Whitney Ellis